This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

include path failing on added file

Hello

I am using CCSv4 with DSP/BIOS 5.41. I had a imported a project from CCSv3.3 successfully and was able to add 2 new files to the project. One of the new files contains an include directive which points to a file in the same subdir as the new (and all) source and header files (flat directory structure).

When I try to compile, I get this: "fatal error #5: could not open source file "utils.h". this include file is included in the other files that were part of the original, migrated project and they compile just fine. Looking at the generated ".pp" files, it shows the migrated files contain the path but the added file's ".pp" file doesn't have the correct path. Comparing the files' build properties, they are the same. The include options are the same on both as well.

Can anyone point out what I've missed?