Other Parts Discussed in Thread: TMS320TCI6488
is there a specific simulator for the TCI6488? and if yes, from where i can download it and how is the installation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320TCI6488
is there a specific simulator for the TCI6488? and if yes, from where i can download it and how is the installation?
TCI6488 simulator is available. You need to have CCS3.3 SR12 service release. SR12 installer is available at:
You need to have CCS3.3 Platinum base installation for this.
If you are trying out CCSv4 already, the simulator is available with that as well. Link to get CCSv4 : http://tiexpressdsp.com/index.php/Category:Code_Composer_Studio_v4
REgards,
Anuradha.
thanks for your answer, but it refused to be installed and gave me a message said that "Setup has not found any valid products to update, your system may already be up-to-date or you are attempting to install a serial update out of sequence, Setup will now abort".
I'm guessing you have CCS 3.3. Do you have the eval or DSK versions? or do you have the full version?
yes you are right, i am using CCS 3.3. (i am sorry for forgetting to mention it [:)]).
and about the version i use, i use the version which comes with the evaluation board TMS320TCI6488 from spectrum digital (i think it is a DSK version).
Hi,
I guess you need to have a full product installation of CCS3.3 to get the SR12 update. The CCSv3.3 that came with the EVM is going to expire eventually.
Are you open to using CCSv4? You could download that from the mediawiki site and if you click the button to use the "Free Limited License". This would enable you to use the sim.
http://tiexpressdsp.com/wiki/index.php?title=Category:Code_Composer_Studio_v4
Regards,
Anuradha.