Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO
I am having a number of problems with my CCS installation with OMAP-L137 EVM.
When I run C:\CCStudio_v3.3\cc\bin\cc_app.exe, I never get past the splash screen. It doesn't seem to matter what my setup is.
I have more success using C:\CCStudio_v3.3\cc\bin\cc_setup.exe -i "C:\CCStudio_v3.3\drivers\import\evmc6747_v1.ccs" -startCCS
However while I can get this to work, any changes I make in Component Manager do not happen. I can only use the components that come with the original install. The Component Manager shows the settings I want, but the CCS About shows the install components. Fortunately using the CCS install from the EVM increased CGTools from 6.0.8 to 6.1.5, fixing a bug I attributed to the compiler.
Also I have other projects I need to maintain, so I'll need more than just the OMAP-L137 EVM setup.
I have uninstalled/reinstalled a couple of times.
I tried running service release 12, and that did not seem to take.
Any suggestions?
Thanks,
Chris