Other Parts Discussed in Thread: UNIFLASH, TMS570LS3137
Hello,
I am using CCS5.x with XDS510USB and the board vendor supplied flash.cmm config file for the Lauterbach debugger. I would like to use CCS5.x with XDS510USB environment for application development. How do I port the contents of flash.cmm which is necessary to flash the application to the target board?
;========================================================================
; Setup CPU
SYStem.RESet
SYStem.CPU TMS570LS3137-ZWT
SYStem.JtagClock CTCK 25MHz
SYStem.MemAccess DAP
ETM.OFF
SYStem.Up
;========================================================================
; Flash declaration
FLASH.RESet
; Program flash
FLASH.Create 1. 0x000A0000--0x0017FFFF 0x20000 TARGET Byte 0. ; Bank 0
FLASH.Create 2. 0x00180000--0x002FFFFF 0x20000 TARGET Byte 1. ; Bank 1
; use flash algorithm with automatic ECC generation
FLASH.TARGET 0x08000000 0x08001000 0x4000 ~~/demo/arm/flash/byte_be/f021r4.bin
FLASH.CLocK auto
;========================================================================
; Flash programming
DIALOG.YESNO "Program application to flash memory?"
LOCAL &progflash
ENTRY &progflash
IF &progflash
(
FLASH.ReProgram 0x000A0000--0x002FFFFF /Erase
Data.LOAD.auto .\build\main.hex
FLASH.ReProgram off
Print "Application flashed..."
)
;========================================================================
; load application symbols
Print "Loading Application symbols..."
Data.LOAD.auto .\build\main.out /noCODE
Print "Application symbols loaded..."
;========================================================================
; breakpoint configuration
; use onchip breakpoints
map.bonchip
;========================================================================
; setup view
; Switch to high level view (only C, no assemler code)
Mode.HLL
; Set format of data values to hex and decimal
setup.var %Decimal %E
;========================================================================
; setup window configuration
DIALOG.YESNO "reset window configuration?"
entry &reswin
if &reswin
(
TOOLBAR ON
STATUSBAR ON
FramePOS 28.125,16.071,,,Maximized
WinPAGE.RESet
WinPAGE.Create P000
WinCLEAR
WinPOS 103.63 0.0 52. 29. 0. 0. W001
Register /Spotlight
WinPOS 0.0 0.0 99. 44. 13. 1. W000
WinTABS 10. 10. 25. 62.
Data.List
WinPOS 103.5 33.143 52. 23. 0. 1. W002
WinTABS 21. 21.
sYmbol.Browse.Function
WinPOS 160.25 0.0 75. 49. 0. 0. W004
Var.Watch
WinPOS 160.25 54.571 77. 5. 10. 1. W005
rt
WinPOS 0.0 49.643 99. 7. 23. 1. W003
WinTABS 0. 0. 0. 0. 0. 0. 0.
Break.List
WinPAGE.select P000
)
; Add reset toolbar
menu.REPROGRAM "bsp\toolbar.men"
;======================
;=== end of script ===
;======================
ENDDO
Thanks & regards,
Krishna