Hello. I'm getting an error in every .c file I have:
fatal error #35: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
Now I have done some searching and tried these commands:
#define -dCHIP_6713
#define "-dCHIP_6713"
#define -CHIP_6713
#define "-CHIP_6713"
And I have done the same in project->properties->CCS Build->C6000 Compiler->Predefined Symbols:
--define="CHIP_6713"
-dCHIP_6713
-CHIP_6713
And so on.
Every one of these attempts gives me this error style:
Command-line error #1046: invalid macro definition: -dCHIP_6713
Could I get a hand in nailing down the command needed to fix this error?
Thanks for your time.