This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding external libray to CCSv5.5

Hi,

I am trying to add external library called armadillo (linear algebra library,www.arma.sourceforge.net) to CCSv5.5, I installed that library in my system (linux) and in CCS project->properties->C6000Compier->include options I gave path to folder under which that library got installed and added .so file and it's path in CCS project->properties->C6000linker->file search path. But when I build project I am getting errors in the header files (.hpp) of the library which I included. Is the way of adding this library properly done? If so why am I getting errors in header files of the library?.  BTW the library I am adding is C++ library.