Hi I am trying to use the SCI port of the 2809 to write to a file on my PC using CCS3.3. When I have CCS3.3 running I am able to create the file on the PC without any problems, but when I stop CCS and try to create the file nothing happens, no file is created. I belevie my code is correct as it works with CCS running, so I am stumped as to why it will no work without CCS. I have tried to following SPRA861 on the device without any success. Thanks
Jorge