This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Champs,
A customer of mine reported a CCSv4 problem similar to and old issue mentioned on the external forum (Oct 09). But there was no answer there:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/3306/11624.aspx#11624
During build they get an "Errors running builder "Generated Makefile Builder" on project occ_dsp." error. The log (attached) shows the following error:
!MESSAGE An internal error occurred during: "Searching for local changes".
It seems to be project related, as some projects can still be compiled without error, but another one not. Reinstalling CCSv4 didn't help. And using an old version of the failing project also doesn't compile. What could be the reason?
Thanks,
Robert
Hi Robert,
Would it be possible to obtain the project? Or at least a stripped down version which could serve as a reproducible test case?
Thanks
ki
If neither is possible, the .project file in the project folder may be enough. We suspect it may be a corrupted .project file.
Thanks
ki