_EVMC6747_init C:\\CCStudio_v3.3\\boards\\evmc6747_v1\\dsp\\tests\\dycfir\\Debug\\main.obj
error: unresolved symbols remain
"main.c", line 57: warning: relocation from function "main" to symbol
"_EVMC6747_init" overflowed; the 31-bit relocated address 0xdfffe580 is too
large to encode in the 21-bit signed PC-Relative field (type = 'R_C60PCR21'
(82), file =
"C:\\CCStudio_v3.3\\boards\\evmc6747_v1\\dsp\\tests\\dycfir\\Debug\\main.obj
", offset = 0x00000008, section = ".text")
error: errors encountered during linking; "./Debug/fir.out" not built
>> Compilation failure
******************************************
what's wrong with the project?