Other Parts Discussed in Thread: CODECOMPOSER, OMAP-L137
Hy, verybody,
I'm new recent user of CodeComposer V3.3.38.2, and I don't succeed to connect to my board...
I have each time following error :
Error connecting to the target:
Error 0x80000220/-2062
Fatal Error during: Execution, OCS,
Cannot halt the processor
Sequence ID: 0
Error Code: -2062
Error Class: 0x80000220
I/O Port = 240
Board Name: ARM9 JTAGjet Emulator
Cpu Name: ARM9_0
I have check emulator and it seems OK... I really don't understand how to debug/solve this problem.
Is there anybody who can hep me please?
Laurent