When using the F021 Flash API 2.01.00 I got the following error for different files:
error #16004-D: file
"../vendor/F021FlashAPI/F021_API_CortexR4_BE.lib<Read.WdService.obj>" has a
Tag_PCS_config attribute value of "1" that is different than one previously
seen ("0"); combining incompatible files
With F021 Flash API 2.00.01 I got no errors.
CCS 5.5.0
F021 API 2.01.00
HalCoGen 4.00.00
TMS570LS3137