This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do TIXDS100 driver for 64+ cpu core of CCS deassert TRST pin??

Greetings,

I have a third party XDS100 emulator which works fine with F2802x (F28xx cpu core) based boards. But the same emulator does not work with a 64+ cpu core based dsp (TCI6486).

I am using 674x CPU core in the target configuration. This is C64+ floating point core.  And as the configuration file of this DSP suggests it is going to use tixds6400_plus.dvr driver.

So the same configuration should work for any 64+ cpu core based cpu. But I am not able to connect to the board.

On the board TRSTn is puled down with a 4.75K resistor, this suggests that it is the responsibility of the emulator to pull it up to bring the TAP controller out of reset.

Does any body have idea whether CCS driver for XDS100 emulator and 64+ core ( tixds6400_plus.dvr) deasserts the TRST pin on connection?

 

Help is highly appreciated..

Thanks,

Amit

amitkumar.solanki@einfochips.com