Other Parts Discussed in Thread: CCSTUDIO
I am having trouble connecting to the cla of the 28035 We I try to connect I get the following error:
Warning:
Error 0x40000202/-1
Warning during: Memory, OCS,
This error was generated by TI's USCIF driver.
SC_ERR_TRIVIAL_NEG <-1>
This '-1' value should be returned only during code development.
It is a temporary value used when a more appropriate error value
has not yet been assigned. This is the most negative of the three trivial
error numbers that are used by USCIF adapters, drivers and utilities.
I/O Port = 0
Board Name: Blackhawk USB2000 - F28035 CLA Controller
Cpu Name: cla_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
I am using
CCS 3.3.83.16
Blackhawk UBS2000 with the following drivers:
Driver Release v3.3.300.2, 23 JUN 2009
CCStudio v3.3 Driver files with USCIF v35.34.0.2 support
This driver will install Blackhawk emulator files for CCStudio v3.3 with SR12 applied. This update replaces all other CCS v3.3 driver releases. No other patches are needed.
Also included in this update are:
-
Updated imports to support the new C2000 Piccolo B F2803x devices.
-
Added C6457 Imports.
SR12 Patches:
-
C2000 CLA Support v3.3.0.0, 24 JUN 2009
Installs only Blackhawk emulation files for CLA support and requires base SR12 driver release above to already be installed on your system.