Hi,
I've downloaded the Code Composer v3.3 Trial Download from the TI website, copied it into a uncompressed folder, and then run 'setup.exe' from its root.
The installer appears to get to the very end before locking up my PC (and I need 2 resets of the PC to get it started properly after that).
Upon restarting my PC it claims to have found new hardware 'TI XD S560 PCI JTAG Emulator' and asks if I want to search for drivers. When I select the 'automatic search' option it finds 'xds560.sys' and tries to install it, gets to the end and locks up my PC.
Restarting again...
After that I have shortcuts for CCS on my desktop (from the above CCS installation) and I can run the CCS Config tool. I select the simulator for the DM642 and I get an error box entitled 'DLL' that states 'an attempt was made to load a program with an incorrect format'. I can still save my settings, but when I try and run CCS proper I just get the same error box.
Looks to me like my PC doesn't like that 'sys' file, but what can I do about it?
All help appreciated. Cheers.