Other Parts Discussed in Thread: LM3S1968, EK-LM3S1968
I'm trying to use the GNU toolchain https://launchpad.net/gcc-arm-embedded/4.7/4.7-2012-q4-major in Code Composer Studio V6. I want to use the Stellarisware drivers, so as a test I am trying to build and run the graphics.c project example from Stellarisware. I can build the project fine using TI's compiler, but I want to setup the GNU ARM toolchain as it is being used on another project.
I have added the compiler, so I have "GNU v4.8.4 (Linaro)" as my compiler version.
I have these under the compiler include paths (-l):
"${CG_TOOL_INCLUDE_PATH}"
"C:\StellarisWare"
"C:\StellarisWare\boards\ek-lm3s1968"
"C:\StellarisWare\utils"
But I am not sure how to setup the linker. So far I have these entries under the Libraries (-l):
"c" "gcc" "nosys"
I have not changed anything else. As expected I am build errors like this when try and build the LM3S1968 "graphics" example project: