This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Could not obtain valid waveform from TI CCS4 graph

Dear all, 

There are issues which prevent me viewing the correct signal. 

Tool used and software: 

Hardware: TI Piccolo F28027 ControlStick

Software: CCS V4.02 

Issue: (Please refer to the picture I posted, I have my graph configuration, watch window and graph listed)

Have issue to view Start Address A (value 100, double) and Start Address B (value 0, double). I could view the value change in the watch list. However, the graph is not correct especially Start Address A . 

Could anyone give me a hand?

Thanks!

  • I tried different Q value, buffer size and data type, but I did not find a good solution 

  • Hi,

    I am unsure what may be happening in this case, but I have some comments/tips:

    - If the variables are double - i.e., floating point, why are you displaying them as 16-bit integers?

    - some of the CCSv4.0 releases had severe issues to display graphs, especially dual graphs. I would be careful using such an old release.

     If the changes to the parameters do not fix the display, you could try to get a CCSv5.5 or v6.0.1 to see if you can load the .out generated from the v4 project and display the graphs properly.

    You can use a newer release without interfering with your previous one if you install CCS in a different directory and use a different workspace. Also, if you import the project, make sure to create a backup copy (CCS projects are not backwards compatible, therefore opening your existing project in a v6 session will render it unusable in v4).

    Hope this helps,

    Rafael