This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Download problem with CCS 6.0 for WIn7 64-bit



I am trying to install CCS for use with a Tiva C Series Launchpad, but the links I have do not seem to provide any option to specify the 64-bit OS.  I killed the firewall and anti-virus and the install ram OK, but the install file is labeled win32 and the config file contains a number of references to Win32, but none to Win64.  I assume that the installed CCS is in fact 32-bit. 

I tried out several of the demo programs on the Launchpad since some other 32-bit applications do work on this system.  The CCS runs OK.  The demos compile and load, but have memory access failures when run. 

My question is how can I locate, download and  install the real 64-bit CCS?