This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Below is the code I'm using to try and print information to the CCE console (CIO). I am following a tutorial, but have been unable to get anything to print. Is there something I'm missing? I am sorry if it does not format properly. Anyone have a suggestion on how to paste code in?
#include
<msp430x22x4.h>
#include
<stdio.h>
void
main()
{
WDTCTL = WDTPW + WDTHOLD;
while(1)
{
printf(
"Hello, World");
}
}
Have you followed the steps outlined in this FAQ, http://tiexpressdsp.com/index.php/CCE_FAQ#How_to_use_printf_in_CCE_v3.3F?
C I/O functions such as printf require a lot of heap space, so as mentioned in the FAQ you would need to increase your heap size within the Project Buid options.
Aarti,
Thanks for the link to the help files. I followed the instructions provided in the pdf but I'm receiving some errors.
The linking failed stating "run placement fails for object ".cio"" and..
"run placement fails for object ".sysmem""
I search for information on these errors and it looks like my target may not enough RAM to support the I/O functions. My target is an MSP430F2274 on the eZ430-rf2500.
Yes that is the likely cause. The F2274 has only RAM size of 0x400 and as you can see from the linker command file (lnk_msp430f2274.cmd), the sections .bss, .sysmem, .stack and .cio are all allocated to RAM. Since CIO functions typically need a lot of heap (.sysmem section) you might be running out of RAM space on the device.
You can create a map file that produces a listing of the input and output sections from the linker where you can review how much space is taken up by each of these sections:
Project-Properties->C/C++ Build -> Tool Setttings -> MSP430 Linker -> Linker Output -> Produce listing of input and output sections in <file> (--map_file)
Hi, Aarti ,
By the way, does this "printf trick" apply to "cout" in C++ 's iostream library?
Br,
AppleCat