Hello, when I am working with CCS in a particular project, I have trouble managing WatchWindow and Memory Registers, i.e., when I am working with them it is very slowly, and for example if I resize the watchwindow to a different shape, it takes long time untill start to respond. Another example, when I switch from a memory register (say McBSP) to another (Core registers) it takes a time too. Similar thing happens when I try to open message log window, it hangs for a while until start to show its values well. What could I check/change to corret this slow behaviour?
Edit: by the way, the project (in fact two projects that has this behaviour) is related with EDMA LLD driver of evmdm6437. I am using CCS 3.3.38.2, and Code genetation tools v6.0.8, and bios 5.31.07
Thanks in advance