Other Parts Discussed in Thread: CCSTUDIO
Hi,
I am running a junit test in CCSv4 as the following:
package example.test.subpackage;
import org.junit.*;
import com.ti.ccstudio.scripting.IScriptSession;
import com.ti.ccstudio.scripting.environment.*;
import com.ti.debug.engine.scripting.*;
import com.ti.dvt.engine.scripting.*;
/**
* Tests for ExampleClass.
* @author testauthor
* @version $Revision 1.10 11 Nov, 2008 First draft <br>
*/
public class ExampleClassTest{
/**
* Test for example method.
* @throws ScriptingException
*/
@Test
public void testExampleMethod() throws ScriptingException {
// Actual test definition
// Create our scripting environment object - which is the main entry point into any script and
// the factory for creating other Scriptable ervers and Sessions
ScriptingEnvironment env = ScriptingEnvironment.instance();
DebugServer debugServer = null;
DebugSession debugSession = null;
try
{
// // Get the Debug Server and start a Debug Session
debugServer = (DebugServer) env.getServer("DebugServer.1");
//debugServer = (DebugServer) env.getServer("CCSServer.1");
//debugServer.setConfig("C:/Program Files/Texas Instruments/ccsv4/scripting/examples/C64/tisim_c64xple.ccxml");
debugServer.setConfig("../scripting/examples/C64/tisim_c64xple.ccxml");
debugSession = debugServer.openSession(".*");
// Load a program
debugSession.memory.loadProgram("C:/Program Files/Texas Instruments/ccsv4/scripting/examples/C64/modem/Debug/modem.out");
}
catch (Exception e)
{
System.out.print(""+e+" Exception catched!!");
}
}
}
The failure trace tells that:
java.lang.ExceptionInInitializerError
at com.ti.debug.engine.cce.CCEDebugEngine$Factory.createInstance(CCEDebugEngine.java:48)
at com.ti.debug.engine.scripting.DebugServer.start(DebugServer.java:612)
at com.ti.debug.engine.scripting.DebugServer$SessionFactory.<init>(DebugServer.java:141)
at com.ti.debug.engine.scripting.DebugServer.openSession(DebugServer.java:1112)
at example.test.subpackage.ExampleClassTest.testExampleMethod(ExampleClassTest.java:46)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.junit.internal.runners.TestMethodRunner.executeMethodBody(TestMethodRunner.java:99)
at org.junit.internal.runners.TestMethodRunner.runUnprotected(TestMethodRunner.java:81)
at org.junit.internal.runners.BeforeAndAfterRunner.runProtected(BeforeAndAfterRunner.java:34)
at org.junit.internal.runners.TestMethodRunner.runMethod(TestMethodRunner.java:75)
at org.junit.internal.runners.TestMethodRunner.run(TestMethodRunner.java:45)
at org.junit.internal.runners.TestClassMethodsRunner.invokeTestMethod(TestClassMethodsRunner.java:71)
at org.junit.internal.runners.TestClassMethodsRunner.run(TestClassMethodsRunner.java:35)
at org.junit.internal.runners.TestClassRunner$1.runUnprotected(TestClassRunner.java:42)
at org.junit.internal.runners.BeforeAndAfterRunner.runProtected(BeforeAndAfterRunner.java:34)
at org.junit.internal.runners.TestClassRunner.run(TestClassRunner.java:52)
at org.eclipse.jdt.internal.junit4.runner.JUnit4TestReference.run(JUnit4TestReference.java:38)
at org.eclipse.jdt.internal.junit.runner.TestExecution.run(TestExecution.java:38)
at org.eclipse.jdt.internal.junit.runner.RemoteTestRunner.runTests(RemoteTestRunner.java:460)
at org.eclipse.jdt.internal.junit.runner.RemoteTestRunner.runTests(RemoteTestRunner.java:673)
at org.eclipse.jdt.internal.junit.runner.RemoteTestRunner.run(RemoteTestRunner.java:386)
at org.eclipse.jdt.internal.junit.runner.RemoteTestRunner.main(RemoteTestRunner.java:196)
Caused by: java.lang.NullPointerException
at java.io.File.<init>(Unknown Source)
at com.ti.debug.engine.cce.DLLPreLoader.<init>(DLLPreLoader.java:20)
at com.ti.debug.engine.cce.ADebugEngine.<clinit>(ADebugEngine.java:45)
... 25 more
What is wrong? The source codes are copied from the http://tiexpressdsp.com/index.php/DSS_from_Java. This prolem is frustrating me a lot.
Br,
AppleCat