Other Parts Discussed in Thread: CCSTUDIO
Hi,
When I try to import a legacy DVSDK 1.11 application I am having several issues:
1) I am seeing a Warning in my project.log when I run the CCSv3.3 import wizard from CCS6:
!WARNING: Unresolved tool: com.ti.ccstudio.buildDefinitions.C6000.Debug.1858260972::XDC
I assume this stems from the following line in the project file?
Tool="XDC"
Is this something to be concerned about or can it be safely ignored?
2) Also, the cmd_file that the compiler looks for is specified as:
cmd_file = "${SRC_ROOT}/=${PROJECT_ROOT}/xdcconfig/compiler.opt"
which produces an erroneous path. I see this regardless of which project I try to install.
Regards,
James