This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS Analyser and CCS6

Hi,

I'm using RTOS analyser to monitor some variables values and CPU load. When it works it is fine but it does not always start or quit properly. Here is a list of the issues I encounter regularly:

  • When terminating the debug sessions, sometimes it closes the RTOS analyser, sometimes not.
  • When starting the debug sessions and the previous RTOS analyser windows still shows, it does not get the values from the board
  • At first I was using the button "Execution Analysis" to launch it. However after 1 day of using it, this button would not work anymore. I then used the button Load analysis to launch it.
  • Sometimes it shows an empty menu, see attached screenshot. 
  • I regularly have to make several trials to make it work

Can you tell me exactly the sequence I have to use to make sure I have no problem?

And how can I reset everything related to RTOS analyser?

I'm using the following configuration:

CCS V6.0.1.00040

UIA 2.0.0.28

EVMDM6437