This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs 5.5 installations issue



hi:

        I use windows 7 (64bits)system,i have been installed ccs 5.3,i can't uninstall ccs5.3 succesfully,so i delate the file,now i want to install ccs5.5 ,but  the installation program prompts me eclipse core correctlly,i have already           up load        InstallJammer Registry  .1541.ccs_setup_5.5.0.00077_install.log0334.ccs_setup_5.5.0.00077_install.log

  • Due to a limitation in eclipse, the username cannot contain any Unicode characters. In order to install the product, please create a temporary admin user and install CCS for all users as adminstrator.

    Best Regards,

    Danish Innis 

  • Thanks for your response! I install the ccs succefully,now here have a new issue,ccs in temporary account normal operation,but in previous account compile error!

  • Hello Su, 

    Could you let me know what type of error you are getting? I.e. what do you see in the build console. Also, are you using the same workspace that you created with temporary user or a new workspace? It might help if attache .log file that can be found in <YourWorkspaceDirectory>/.metadata folder. If you don't know the workspace location then the quickest way to find out is to click on File->Switch Workspace->Other, the dialog that pops up will show the current path to workspace. You can then cancel out of the dialog. 

    Martin