I'm running a new install of CCSv5.5 and connecting to a new Spectrum Digital XDS200 USB emulator. My target board is running a TMS320C5502 processor.
When I run Test Connection immediately after connecting the emulator USB cable to my Win 7 laptop, it runs successfully. Subsequent Test Connections reveal the following error:
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
If I switch USB ports, The first Test Connection works, and then I get the same error on subsequent tries.
I also have CCSv5.5 running on an XP desktop, and with the same cable, emulator and target, Test Connection is successful every time.