Other Parts Discussed in Thread: TM4C1294NCPDT
Using CCS 6.0.1.00040 when a new project was created for a TM4C1294NCPDT using the GNU v4.7.4 compiler, noticed there were errors in the generated project which caused run time failures. E.g. using a project containing the following code:
/*
* main.c
*/
#include <string.h>
char test_string[20] = "Hello World\n";
int main(void) {
volatile size_t len = strlen(test_string);
return 0;
}
The first problem is that the data segment has not been initialized correctly. E.g. the text in the test_string appears offset by 12 bytes:
The incorrect data segment initialization is caused by the tm4c1294ncpdt_startup_ccs_gcc.c added to the project by CCS. The error is that the ResetISR() function uses __etext as the source of the data segment initialization, whereas it should be using __data_load__. i.e. change the tm4c1294ncpdt_startup_ccs_gcc.c to contain:
//*****************************************************************************
//
// The following are constructs created by the linker, indicating where the
// the "data" and "bss" segments reside in memory. The initializers for the
// for the "data" segment resides immediately following the "text" segment.
//
//*****************************************************************************
extern uint32_t __data_load__;
extern uint32_t __data_start__;
extern uint32_t __data_end__;
extern uint32_t __bss_start__;
extern uint32_t __bss_end__;
//*****************************************************************************
//
// This is the code that gets called when the processor first starts execution
// following a reset event. Only the absolutely necessary set is performed,
// after which the application supplied entry() routine is called. Any fancy
// actions (such as making decisions based on the reset cause register, and
// resetting the bits in that register) are left solely in the hands of the
// application.
//
//*****************************************************************************
void
ResetISR(void)
{
uint32_t *pui32Src, *pui32Dest;
//
// Copy the data segment initializers from flash to SRAM.
//
pui32Src = &__data_load__;
for(pui32Dest = &__data_start__; pui32Dest < &__data_end__; )
{
*pui32Dest++ = *pui32Src++;
}
The second problem is that the strlen function was crashing the processor - causing the FaultISR() to be entered. This is because the strlen function was being linked from the c:/ti_ccs6_0/ccsv6/tools/compiler/gcc-arm-none-eabi-4_7-2013q3/bin/../lib/gcc/arm-none-eabi/4.7.4/../../../../arm-none-eabi/lib\libc.a library. That library has been compiled for ARM mode, whereas the TM4C1294NCPDT device only supports Thumb mode.
The incorrect library being linked is caused by the GNU compiler -march option being left blank when the project was created by CCS. -march should be set to "armv7e-m" for a TM4C1294NCPDT to cause the GNU compiler to select the correct run time library.
With these two changes the above example then worked when compiled with the GNU v4.7.4 compiler