Other Parts Discussed in Thread: SYSBIOS
CCSv5.5, Windows 7, XDS560v2 Spectrum Digital, Spectrum Digital Emulators 5.2.0.12, C6472, CGT 7.2.6, SYSBIOS 6.35.4.50, XDCtools 3.25.3.72, IPC 1.24.3.32
Hi
After setting breakpoints in my code, I can select run and CCS stops at the breakpoint. But after reload, its seems random whether or not the breakpoints will be hit.
The little blue icon on the left column is still present when I view the code.
I've ensured I'm using the HW breakpoints.
Deselecting and then re-selecting the breakpoint in the view->breakpoints tab does not appear to consistently work.
The only solution I've found is to manually toggle the breakpoint by double clicking on the left hand column in the edit window.
The breakpoints worked fine in CCSv4.
I've built my code to run on only two cores. I've "grouped" the two cores and select the "Group 1" to do the reload.
Optimizations are disabled for the file containing breakpoints.
Any thoughts, suggestions, fixes, patches, ideas on how to get this working like CCSv4?
(my colleagues also see the same issue)
Cheers2u
Eddie