I fired up CCS4 v. 4... don't remember what number. Got an alert about an update being available. Ran with that. Was told CCS would have to restart. Did that. There was some cryptic message, presumable from Windows, saying "Application corrupt", but CCS did restart. It is now showing v.4.1.0.0100.
Go to File/New/Other. Get Select a Wizard dialogue. It is dead, cannot select anything, hence cannot create a new file.
Machine is a Dell Precision M64000 running WIn XP x64 Professional, SP2, 8 GB RAM
Any idea what's wrong? Should I just reinstall CCS4 from scratch? Where from in that case?
/Paul