This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 3.3 doesn't generate hex file

I have a legacy project that requires a modification.

It is coded in CCS3.3.

I can build in debug mode, and generate an .out file.  However no .hex, or .bin is being generated.

I have looked over the posts on compiler installation and can confirm that the C6000 tool is present in the program. 

Can you help me generate a hex or binary file?

Thanks.