Hi,
I am working on a DSP project previously built on CCS 2.20, which I am trying to build using CCS 3.3 now. On opening the project in CCS 3.3, the CDB2TCF utility converted the DSP/BIOS Configuration file from CDB to TCF format. But the project has a Visual Linker Recipe file(.rcp) for linking and it is not recognized in CCS 3.3. The rcp file is displayed under the Documents in the project Window. I came to know from the below links that Visual Linker is not supported from CCS3.0 onwards.
https://community.ti.com/forums/p/5055/18635.aspx#
Please let me know if there are some tools or mechanisms available to generate a .cmd file from the .rcp file so that I can use it for linking.
Or are there any guidelines available on how to include details in the .rcp file in to the .tcf file?
Regards
Shiras