Hi,
I have a project that includes both algebraic and mnemonic assembly language source files. I am using the C5505 USB100 stick and CCE 4.0 to compile the project. I am getting parsing errors and no object file because of the two different types of assembly code in the project. Is there a way of selecting the build options on a per file basis? If not then is there a way I can choose both algebraic and mnemonic options to build the project?
If there is not a setting in CCE4.0 that will allow me to build using both options, please suggest an alternative without me having to convert one set of files to either mnemonic or algebraic.
Thanks,
Arthi Bhat
Acoustic Acuity Inc.