This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Giancarlo,
Other than maybe some CGT entries, CCSv4 should not be using the Windows registry. You shouldn't have to do registry cleanup after uninstalling ccsv4. Usually just dealing any left over files in the folder is enough. The only issue with installing another CCSv4 install is if you try to install over an existing install (same directory).
The compiler.reg... that was to add registry entries as needed by 3.3. I think they come with v4 but I don't think it is necessary for them to run? I'll need to check on that...
ki
Hi Ki,
below the last feedback from the customer on this:
CCSv4 is using the registry because I find references to it there. The compiler.reg files refer to CCSv4 so I assume they are required.
If I install without executing these manually then CCS will not compile files but with no notification of this.
The above has now cost me at least a day installing & reinstalling numerous times and debugging your install. I just want to get on and develop some code for which I may get paid by the customer, not just get late on the project because of these simple issues :-)
Perhaps it would be useful if the issues I have found could be fixed so others do not have the same problems. I still cannot install CCS in its default folder on this machine.
Those registry entries are only needed for 3.3. The reason why they show up for v4 is that we are using the same CGT installers that we use for 3.3.
Regarding the issue with detecting the existing install... there must be some leftover install files. Sounds like they had some install failures in the past or did something not recommended (like installing over an existing install).