Other Parts Discussed in Thread: TMS320VC5506
Hello,
Due to budgetary constraints, my client purchased an XDS510 USB 2 device on eBay. It came with no documentation other than a CD-R with several conflicting files. I was able to get this XDS510 working last year with our custom board on a borrowed PC running CCS3, but I did not take notes on which driver was successful, and now I do not have access to that machine any more. We're now trying out CCSv4 with the XDS100 on our own Window XP machine, but I find it slow and buggy, and would like to try the XDS510 again, with CCS3 and CCSv4, if possible.
Can anyone help me identify this XDS510 hardware?
The USB VendorID is 0x0B1E "Electronic Warfare Assoc., Inc. (EWA)", the ProductID is 6, and the Device Version Number is 2.0.0 (0x0200)
The circuit board says "TI DSP Emulator" XDS510-usb2.0 KG0901-12Y180K and has chips including ACT8990, Cypress CY7C68013A-100AXC, Lattice B832KK08 and a 24 MHz crystal, among other parts.
My problem is that I can't seem to figure out which drivers to install, since there are about 3 different drivers on the CD-R. If I knew for sure who made this hardware, and which driver was appropriate, then I'd probably be able to get it working. Last year, I struggled with strange error messages and was working with an unproven TMS320 board of my own design, but eventually got it working. If only I had realized that I would of course forget which driver and settings worked, then I would have taken careful notes.
P.S. Another issue is that I "improved" our TMS320VC5506 board by adding pull-ups on the JTAG header, so I cannot even be certain that I didn't make things worse. Obviously, narrowing down the possibilities by removing variables is going to be key. I still have the old boards, though, if that turns out to be the issue.