This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help on Warning #64-D Shift count is too large



Hello,

The hardware I am working with is a 5502 DSP with Micron M25P80 serial flash.

The software is Code Composer Studio Version 5.1.1.00031

Problem: I am reading the boot table from a .bin file stored in flash.  I read the first four bytes of the file (32 bit entry point) and I want to assemble the bytes into a uint32_t. I use the following code to achieve this and receive the "Warning #64-D Shift count is too large" message.

Code Snippet

 // Get the entry point for the binary file being loaded

// The entry point is in the first four bytes of the Boot Table
entryPoint = spiflash_read_byte(flash_offset++) << 24;
entryPoint = entryPoint + spiflash_read_byte(flash_offset++) << 16;
entryPoint = entryPoint + spiflash_read_byte(flash_offset++) << 8;
entryPoint = entryPoint + spiflash_read_byte(flash_offset++);

End Code Snippet

Below is the code snippet that reads the flash:

Code Snippet

unsigned short spiflash_read_byte(unsigned long int flash_offset)
{
unsigned short ret_val;

assert_chip_select();

// Send READ command
while ( (MCBSP0_SPCR2 & BIT1) == 0 ) {} // wait for XRDY
MCBSP0_DXR1 = READ_CMD;
while ( (MCBSP0_SPCR1 & BIT1) == 0 ) {} // wait for RRDY to indicate write completed
MCBSP0_DRR1; // throw away dummy data

// Send address[23:16]
while ( (MCBSP0_SPCR2 & BIT1) == 0 ) {} // wait for XRDY
MCBSP0_DXR1 = flash_offset >> 16;
while ( (MCBSP0_SPCR1 & BIT1) == 0 ) {} // wait for RRDY to indicate write completed
MCBSP0_DRR1; // throw away dummy data

// Send address[15:8]
while ( (MCBSP0_SPCR2 & BIT1) == 0 ) {} // wait for XRDY
MCBSP0_DXR1 = flash_offset >> 8;
while ( (MCBSP0_SPCR1 & BIT1) == 0 ) {} // wait for RRDY to indicate write completed
MCBSP0_DRR1; // throw away dummy data

// Send address[7:0]
while ( (MCBSP0_SPCR2 & BIT1) == 0 ) {} // wait for XRDY
MCBSP0_DXR1 = flash_offset;
while ( (MCBSP0_SPCR1 & BIT1) == 0 ) {} // wait for RRDY to indicate write completed
MCBSP0_DRR1; // throw away dummy data

// Read Byte
while ( (MCBSP0_SPCR2 & BIT1) == 0 ) {} // wait for XRDY
MCBSP0_DXR1 = 0; // dummy write
while ( (MCBSP0_SPCR1 & BIT1) == 0 ) {} // wait for RRDY to get data
ret_val = MCBSP0_DRR1;

deassert_chip_select();

return ret_val;
}

End Code Snippet

The original "spiflash_read_byte" returned an int.  I changed it to a short, but still get the warning.

While debugging this, it looks like "entryPoint = spiflash_read_byte(flash_offset++) << 24;" is trying to shift a 16bit value into "entryPoint".

If I try the equivalent of this code in Microsoft C, it works as expected.

Any suggestions would be appreciated.

Thanks,

Stephen

  • Stephen Davis said:
    While debugging this, it looks like "entryPoint = spiflash_read_byte(flash_offset++) << 24;" is trying to shift a 16bit value into "entryPoint".

    That's correct.  spiflash_read_byte returns an unsigned short.  That's a 16-bit type on C5500.  It is not legal to shift it more than 16 bits.  I think you mean to write ...

    entryPoint = (uint32_t) spiflash_read_byte(flash_offset++) << 24;

    Moreover, I recommend you use type names like uint32_t and uint16_t throughout this code.  By making your programming intent clear, you avoid problems down the road.

    Thanks and regards,

    -George

  • Hi George,

         Thanks... Your suggestion was spot on!  Everything works as expected now.

    Stephen