I migrated a CCS 3.3 to CCS 5.5. I did it manually as a New Project. I added the files and added the .tcf. Adding the .tcf caused the project to convert to RTSC capable after prompting to notify the user.
I got the project to compile, program, and run. I checked into StarTeam revision control. I went to another PC and checked it out and imported into CCS 5.5. I got the following error:
-------------------------------------------------
This project was created using a version of DSP/BIOS tools that is not currently installed: 5.42.1.09. Please install the DSP/BIOS tools of this version, or migrate the project to one of the supported versions.
-------------------------------------------------
I closed and deleted the project selecting the option to delete from disk as well. I closed CCS 5.5. I checked the files out of RCS again.
I downloaded and installed DSP\BIOS 5.42. I still had the same issue. I went through the steps again, close & delete project with delete disk contents and then close CCS 5.5.
I re-installed the DSP\BIOS 5.42. I rebooted the PC. I imported the project again. I get the same error.
I selected the CCS option to discover new installations on Startup. Same issue after import.
I found this:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/209452.aspx?pi296443=2
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/49056.aspx
But those didn't give a clear answer for my case.
What do I need to do to get CCS to recognize my DSP\BIOS installation?
Regards,
Jim