This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5.5 and XDS510 USB Support

Other Parts Discussed in Thread: OMAP-L138

I'm working with the OMAP54xEVM, and I'm trying to debug the C64x+ DSP core using the XDS510 USB emulator. When setting the connection type, the XDS510 USB option is not available from the drop down. Is this emulator not supported for the OMAP54x and/or CCSv5.5?

All emulator packages are up to date, and I see "SD510USB_Connection.xml" in .\ccsv5\ccs_base\common\targetdb\connections. 

Thanks!