Other Parts Discussed in Thread: TMS570LS20206, CCSTUDIO
Hello,
we are going to develop an electronic board using the TMS570LS20206 microcontroller. We also need a proper JTAG emulator.
(We have already developed in the past using C2000 mcu's and CCS v.3.3.)
1) Is it possible to use CCS v.3.3 with TMS570LS20206? When I open "Setup CCStudio v3.3" and select family "CORTEX-R4", I cannot see TMS570LS20206... Which emulator should I select?
2)If we decide on CCS v.5, is it possible to realize a product using the free downloaded version, or do we have to purchase a version of CCS v.5?
3) With CCS v5, which emulators can be used? On the page: http://www.ti.com/product/TMS570LS20206/toolssoftware I have seen that XDS200 is suggested, but I cannot see it in the list of available connections under CCS v5 free edition...
Thanks for your help,
Elena B.