This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GNU gcc 4.9.1: undefined symbol _end



I'm porting code written from mspgcc 4.6.3 into a CCS 6.0.1 project with TI mspgcc  4.9.1.

MSP430FR59xx is the MCU type.

When linking the symbol _end (as I can read from the code it is the start of RAM + sizeof(data) + sizeof(bss) ) is undefined:

./cpu/msp430-common/msp430-main.o:(.data+0x0): undefined reference to `_end'
collect2.exe: error: ld returned 1 exit status

What symbol name instead of _end I have to use for gcc 4.9.1?

below the code snippet:

extern int _end;        /* Not in sys/unistd.h */
static char *cur_break = (char *) &_end;

#define asmv(arg) __asm__ __volatile__(arg)

#define STACK_EXTRA 32


/*
 * Allocate memory from the heap. Check that we don't collide with the
 * stack right now (some other routine might later). A watchdog might
 * be used to check if cur_break and the stack pointer meet during
 * runtime.
 */
void *sbrk(int incr)
{
    char *stack_pointer;

    asmv("mov r1, %0" : "=r"(stack_pointer));
    stack_pointer -= STACK_EXTRA;

    if (incr > (stack_pointer - cur_break)) {
        return (void *) - 1;    /* ENOMEM */
    }

    void *old_break = cur_break;
    cur_break += incr;
    /*
     * If the stack was never here then [old_break .. cur_break] should
     * be filled with zeros.
    */
    return old_break;
}

Greetings

Attilio

  • I cannot find where this detail is explained in the documentation.  I think the symbol name is "end".  That is because I looked at some executables with the names utility.  The command could look like ...

    % msp430-elf-nm -n executable_file | less
    

    Search for "end".  I expect you will only find "end" and never "_end".  The -n option sorts the output by address, so you can see, based on the names of nearby symbols, whether the address makes sense for your system.

    Thanks and regards,

    -George

  • Thanks George!

    It make sense and seems reasonable that the end symbol is the right address, but ...

    for confirmation I made this simple case:

    #include <msp430.h>
    
    /*
     * main.c
     */
    int main(void) {
        WDTCTL = WDTPW | WDTHOLD;	// Stop watchdog timer
    
        return 0;
    }
    

    then:

    $ msp430-elf-size.exe e2e-post.out
       text    data     bss     dec     hex filename
        582     146      18     746     2ea e2e-post.out
    

    So I expect end = 0x1c00 + 146 + 18 = 0x1ca4

    but instead

    $ msp430-elf-nm.exe -n e2e-post.out
    00000012 A __bsssize
    0000007e A __romdatacopysize
    00001c00 D __datastart
    00001c00 d __JCR_END__
    00001c00 d __JCR_LIST__
    00001c02 D __dso_handle
    00001c04 D _impure_ptr
    00001c06 d impure_data
    00001c7e B __bssstart
    00001c7e D _edata
    00001c7e b completed.2761
    00001c80 b dtor_idx.2763
    00001c82 b object.2776
    00001c90 N end
    

    from nm  outuput end is 0x1c90, not 0x1ca4.

    What I miss?

    regards

    Attilio

  • That's because "end" marks the end of the .bss section.  0x1c7e + 0x12 = 0x1c90.

    Thanks and regards,

    -George

  • The "data" column from the "size" program apparently includes more than what you're considering data.  I played around with some GCC executables, and it seems that (_edata-__datastart) is the size of the .data section only; there are other data sections. 

    Try using the "-A" argument to msp430-elf-size.exe for a more detailed section listing.

    Looking at the output of "nm", we see that (end-__bssstart) is 18, as expected, and (_edata-__datastart) is 126.  This leaves 20 extra bytes unaccounted for in the "data" column of the "size" program.  Possibly const data?

  • It looks like the "data" column is the total size of all writable data sections including .data, but excepting .bss.

  • Ok, data section reported by msp430-elf-size is the sum of .data (RAM) and .rodata (ROM) data:

    $ msp430-elf-size.exe -A e2e-post.out
    e2e-post.out  :
    section                     size    addr
    __reset_vector                 2   65534
    .rodata                       20   17408
    .text                        580   17428
    .data                        126    7168
    .bss                          18    7294
    .MP430.attributes            322       0
    .comment                     123       0
    .debug_aranges               400       0
    .debug_info                 6233       0
    .debug_abbrev               1149       0
    .debug_line                 2370       0
    .debug_frame                 156       0
    .debug_str                  1823       0
    .debug_loc                   563       0
    .debug_ranges                120       0
    .debug_line.text.__errno      22       0
    .debug_line.text.memmove      64       0
    .debug_line.text.memset       34       0
    Total                      14125
    

    Thanks again!

    Attilio