This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to open WorkSpace using CCS-5.5 on 64-bit Windows 7



Hello,

 I had no problem at all in opening workspace using CCS up to 5.4 on Windows XP for years.

Now I have to upgrade to 64-bit Windows 7 due to IT policy at work.

I also install CCS-5.5, just because I don't want to take risk using CCS-6.

I was able to open a new work-space right after installation.

Now I'm NOT able to open that work-space, even worse, I'm NOT able to create any work-space, no matter where it is, even after reboot PC

What should I do ?