This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 FAUCR not showing DIV0 set in test program

Hi,
I am writing a test program for C6678, the test program checks for DIV0  below:
 
extern __cregister volatile unsigned int FAUCR;
void testDIV0(void)
{
  double a = 1, b = 1, c = 0;
  c = 0;
  b = 1 / c;
  printf("\nFAUCR = 0x%x", FAUCR);
}
I expect to see DIV0 in FAUCR set, but the output I get is:

FAUCR = 0x800000
Why is FAUCR not showing  DIV0? How do I perform tests to enable FAUCR to flag out the exceptions such as
underflow or overflow, the rounding mode, NaNs, denormalized numbers, and inexact results?
 
Thanks!