Hi All,
What does "ISA" revision mean on this TI compiler Wiki?
http://processors.wiki.ti.com/index.php/Compiler/diagnostic_messages/16008
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISA is instruction set architecture, which means a processor family such as C6000 or MSP. The family is further subdivided into what are sometimes called revisions. For MSP, the main division as far as the compiler is concerned is MSP vs. MSPX. MSP is a strictly 16-bit device, and MSPX supports an 24-bit address space, which means it has extra instructions to access this address space, as well as other improvements.