This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tiobj2bin missing in CCS6

Genius 5820 points

Hi,


I reinstalled CCS6 for Linux and now are no longer able to build my projects because tiobj2bin is missing. /opt/ti/ccsv6/utils does not contain it. Then I found a package cg_xml where TIs website stated it contains tiiobj2bin but that's not true, after installing it it is still not available, also this package did not contain it.


So how can I get back this tool?

  • Hi,

    It should come with CCS (I see it in my CCSV6 Linux installation). However it might be tied to a particular family install. Did you install the ARM components?

    thanks

    ki

  • Hi,

    I just replied to someone else with the same issue; which devices did you install?

    This bug was present in some releases of CCSv5, and it seems to have returned.

    In the meantime, please check attached a tar.gz. file that contains both the tiobj2bin and mkhex4bin (disclaimer: this file is distributed under the same licensing terms agreed upon the CCSv6 installation).

    Hope this helps,

    Rafael

    tiobj2bin.tar.gz
  • OK, I found the old thread - and the solution is still the same, one have to install the Stellaris-components to get these data.

    I installed Sitara-Package only which resulted in this incomplete installation.

    Thanks!

  • Hi,

    Thank you for reporting this. I filed today the bug SDSCM00051102 and you can check its status in the link SDOWP in my signature below.

    Regards,

    Rafael