Other Parts Discussed in Thread: MSP430F2410
I have IAR to CCS ported code.
I can able to compile the code without any warnings. MCU :MSP430F2410
IDE: CCS V.6.0.1.00040
When i try to flash(debug mode) the code, it is giving me the below error
When i create a simple new project like below it is flashing without any problem.
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
while(1);
return 0;
}
What are the possibilities of this issue..