Other Parts Discussed in Thread: MSP430FR5969, CCSTUDIO
Hi,
I am using Code Composer Studio version 6.01.00040, developing with the MSP430FR5969.
I have had no problems with development thus far until I downloaded the update to the MSP430 Emulators. When I updated to version 6.0.1.5 of the MSP430 Emulators I now receive the following error message whenever I try to download my program to the MSP:
Error initializing emulator: Error loading msp430.dll. Please make sure that the file exists (C:\TI\ccsv6\ccs_base\DebugServer\drivers\msp430.dll)
I can confirm that the msp430.dll file does exist in that location. I have performed a number of re-installs of CCS and was able to pinpoint the problem to the update to the MSP430 Emulators.
Is there anything I can do to fix this? For the time being, I am going to re-install and ignore the MSP430 Emulators update.