This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6 - upload to MSP430 via MSP-FET430-UIF is very slow

So far I worked with CCS5.3 on windows7. Now I have updatet to CCS6. The problem is:

The transfer time of the code from CCS to the MSP430-MCU via the MSP-FET430-UIF is very slow. The transfertime is now round 9 minuts for round 5 KBytes. So far it ward round 2 secounds.

I test ist with the TI-Compiler and with GNU. It is the same.

Could some body help me? Is it possible that I have make a deinstallation of CCS5.3 bevore the installation of CCS6? Have I to change the USB driver for the MSP-FET430-UIF? --> The firmware of the MSP-FET430-UIF is updated automaticly from CCS6.

I haven't found this problem in the ccs forum.