This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x PINMUXTOOL pin assignment

Guru 15520 points

Hi,

I have a question about AM437x PINMUXTOOL-v3.

When I only select GPMC, there are many pin conflict.
The configuration of tool are as following:
Add only one GPMC
 select Use case : Multiplexed 16b NOR Type
 IO Set : GPMC_IOSet_26 (This is selected automatically and user never can change to other IO set)

Why it gets pin conflict by selecting one GPMC which IO set get configured automatically? 
What is the best way to remove pin conflict?
How to select IO set by user?

best regards,
g.f.