Other Parts Discussed in Thread: TMS320C6748
I'm working with CCSv4.1.1 and the LogicPD EVM board for the TMS320C6748. I need to tell the linker to store some data in the off-chip, external memory. I believe this is to be done in the linker command file (linker_dsp.cmd). However, I do not understand the commands in the linker command file.
I'm guessing I must change this:
.far > shared_ram
to this:
.far > external_ram
But that is merely a guess. The trouble is that I cannot find help files on this issue (i.e., on the linker command file). When I search the help files, it either comes up with nothing, or when a topic looks profitable, it responds with:
The topic that you have requested is not available. The link may be wrong, or you may not have the corresponding product feature installed. This online help only includes documentation for features that are installed.
In other words, CCS doesn't give any help on this topic -- the linker command file. (Could it be because I'm using the EVM version of CCS, which is free? In other words, is the EVM version brain-damaged, limited, or otherwise restricted in some way that could explain its above message?)
Where do I find help on this topic? Thanks for your help.