I installed CCS4 about a month back to start work with a new library.
Anyways, I have no problem compiling under CCS4, but trying to get the emulator to work reliably is almost impossible. I have 2 emulators, both Spectrum Digital: XDS510USB and XDS510PP Plus. Both are version A models and both show similar problems. The USB model (at the moment) will not connect at all.
The Parallel Port version connects fine, but always throws some error trying to load the code into memory.
I’m running CCS4 Version 4.1.1.00014 and the newest SD drivers.
I’ve included the log, maybe it will give you an idea to what’s going on ….
The hardware is the same as I have been running for about 5 years, so I know that is not at fault. Also, if I switch back to CCS 2.2 I have no problems whatsoever.
In case you were wondering, I have both CCS 2.2 and CCS 4 installed on this machine. I really hope this is not a problem.
Then, I thought CCS v2.2 and V4 may interference each other on the same computer. I’ve installed CCS4 on a clean laptop. (4.1.0.02006) This fails pretty much the same way as other machine. Just upgraded to 4.1.1.00014, a little different now, it looks like the code loads, but never gets to main. (I’ve also seen this on my other machine) I can only test the XDS510USB, there is no parallel port on the laptop. Thanks!