Hi,all
I am using CCS4.1 to develop omap3530 programe.
In my CCS build setting, the Output Format is set to "eabi (ELF)",
my question is how to make the output format to ".bin" format
which can run in the ram directory.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are you building for the ARM or the DSP?
If you are building for the ARM and you want to generate an executable that can be run from Linux you need to use an appropriate ABI, I am under the impression the EABI setting you have is suitable, but I have never tried doing this. Alternatively you could build with another tool set (i.e. Code Sourcery GNU) that I am certain supports Linux executables.
I will move this thread over into the CCS forum for further comment.
Bernie,Thanks for your reply:)
I am building the ARM programe.
I hava solve the problem by using "tiobj2bin.bat" to make a bin file.
"tiobj2bin.bat" locate "\Texas Instruments\ccsv4\utils\tiobj2bin"