Our software contains a large 2d array. Because of this array, not all cinit data is loaded to the .bss sections. Below is a description of the problem.
Using: TMS320C55x C/C++ Compiler v4.4.1
problem.c contains only:
char foo[3][0x4100] = {{1},{1},{1}};
cl55 -ss -al -v5502 problem.c
This generates 1 .cinit fields, which contain no data. In the .lst file, 3 .sect ".cinit" are created (I would expect there would be 2 in total).
From the list file:
35 000000 .sect ".cinit"
36 .align 1
37 000000 0002 .field $C$IR_1,16
38 000001 0000- .field _foo+0,24
000002 0000
39 000002 0000 .field 0,8
40 000003 0001 .field 1,16 ; _foo[0][0] @ 0
41 000004 0005 .field 5,16 ; _foo[0][1] @ 16
42 $C$IR_1: .set 2
43
44 000005 .sect ".cinit"
45 .align 1
46 000005 0000 .field $C$IR_2,16
47 000006 003F- .field _foo+16383,24
000007 FF00
48 000007 FF00 .field 0,8
49 $C$IR_2: .set 0
50
51 000008 .sect ".cinit"
52 .align 1
53 000008 0001 .field $C$IR_3,16
54 000009 0041- .field _foo+16640,24
00000a 0000
55 00000a 0000 .field 0,8
56 00000b 0001 .field 1,16 ; _foo[1][0] @ 266240
57 $C$IR_3: .set 1
From line 44 to 49 ($C$IR_2), no data is inserted. I experimented with length and data, but the compiler seems always to add this without data. The offset to foo is always 0x3FFF. This offset doesn't change when the size is changed or when more data is inserted.
Run time, this causes a problem with loading the .cinit. From the map file I checked the location of this specific .cinit section. With the debugger, I checked the actual memory. There I discovered that section $C$IR_2 is placed in cinit, but with a length of 0(!). The function which loads cinit (auto_init) stops when it finds a length of 0. This means none of the .cinit after this specific location is loaded.