Other Parts Discussed in Thread: CCSTUDIO, CC3200, CC2650
The title says it all. Has anyone been able to install 5.2.0 with CCS? Is there an installation log? All I get is a license agreement and then "Failed to install the selected add-ons".
Randy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The eclipse log file says:
!ENTRY com.ti.ccstudio.p2app 4 0 2014-12-17 19:58:42.289
!MESSAGE The installable unit com.ti.cgt.tms470..*.win32.feature.group.* has not been found.
But, I installed it using "Install New Software...". However, when I switched to 5.2.0 and recompiled I get:
#10269 output file "dvf.out" exceeds code size limit
The help for 10269 says that I can only use 16 KB on the MSP430 - but I'm using the CC3200. OK, I suppose the
help is wrong. It's an ARM compiler after all and I wasn't using even half of memory before. When I look at
installed software I would think that it should show only the latest version, but I see both 5.1.9 and 5.2.0. I also
have 5.1.6 and 5.1.8 installed.
Oh! A further message in the log. To continue from where I left off:
!SESSION 2014-12-17 20:08:55.880 -----------------------------------------------
eclipse.buildId=4.3.0.M20130911-1000
java.version=1.6.0_13
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Framework arguments: -product com.ti.ccstudio.branding.product
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.ti.ccstudio.branding.product
!ENTRY org.eclipse.equinox.p2.repository 4 0 2014-12-17 20:09:10.063
!MESSAGE An error occurred while downloading http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/codegen/Updates/p2linux/content.jar. The cache file C:\ti\ccsv6\eclipse\p2\org.eclipse.equinox.p2.repository\cache\downloading\content-849959563.jar could not be renamed to C:\ti\ccsv6\eclipse\p2\org.eclipse.equinox.p2.repository\cache\downloading\content-849959563.jar.
I'm back in business with 5.1.9.
Randy
It was my understanding that the code size limit only applied to the TI MSP430 compiler.Randy John said:The help for 10269 says that I can only use 16 KB on the MSP430 - but I'm using the CC3200. OK, I suppose thehelp is wrong. It's an ARM compiler after all and I wasn't using even half of memory before.
However, there is this post http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/p/389740/1377017#1377017 that reports that the TivaWare freertos_demo for the DK-TM4C129X:
- Compiles successfully with the TI ARM 5.1.9 compiler
- If use the TI AM 5.2.0 compiler the linker fails reporting the error:
Running CCS 6 under Linux I found that:<Linking>
error #10269: output file "freertos_demo.out" exceeds code size limit
error #10010: errors encountered during linking; "freertos_demo.out" not built
- The TivaWare freertos_demo for the DK-TM4C129X successfully compiles and links when the TI ARM 5.1.9 compiler is used with a free license.
- The TivaWare freertos_demo for the DK-TM4C129X fails to link when the TI ARM 5.2.0 compiler is used with a free license, with the linker reporting "error #10269: output file "freertos_demo.out" exceeds code size limit".
- The TivaWare freertos_demo for the DK-TM4C129X successfully compiles and links when the TI ARM 5.2.0 compiler is used with a full license.
Therefore, it appears that the TI ARM 5.2.0 compiler has imposed a code size limit when a free license is used - not sure if this was intentional.
Edit: Correct compiler versions
JohnS said:Randy,
What is happening is a release timing issue. There is a code size limit in the 5.2.0 compiler, it is not supposed to apply to CC3200 but the logic that controls what devices it applies to is in CCS and the CCS update with that logic isn't out yet and the compiler release is. I am going to send you a friend request. Once that is setup I can send you a private message with a workaround.
Regards,
John
I am experiencing the exact same issue, can you put a workaround up?
Jakob,
I will send you a private message with a special license file that will workaround this issue until CCSv6.1 comes out.
Regards,
John
Hi all,
i am facing a problem related to the installation of TI ARM compiler 5.2.6 for compilation of programs to be operated in CC2650 Launchpad.